Part Number: UCC29002
Tool/software:
Hello Team,
I am using UCC29002 LOAD share IC for my converter,the output load current is 8.33A,The problem is when change the load current from full load to lower load that is till 1A the load sharing is proper in terms of DC rms current but when observed the load current waveform ,it is DC current which is proper till 5A but when i reduce the load current below the 5A the current pattern is noisy but the DC rms current measured is equally shared among the two converters,the gain set is 100,and sense resistor is 3mohm,even when i increased the sense resistor value or the gain there is no change in the behaviour.could you help me to fix the issue i have attached the current waveforms captured at different load currents for your reference12V Variant paralleing current waveforms.docx