This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: BQ76952 COV Triggering Below Threshold

Part Number: BQ76952

Tool/software:

Hi TI team,

We are using the BQ76952 in our design and encountering an issue with the COV protection.

The COV threshold is configured at 4199.8 mV, but the protection flag is being set when the cell voltage reaches only 4167 mV.
We have already calibrated the voltage, and both the actual cell voltage and the ADC reading are aligned and accurate.

Could you help us understand what might be causing the COV to trigger below the set threshold?
Is there any additional setting or margin that we might have missed?

Thank you in advance for your support!

Best regards,