Other Parts Discussed in Thread: TPS74801EVM-177,
Tool/software:
The TPS748A datasheet on the first page notes:
Stable with any output capacitor >= 10 uF
which is also reflected in table "6.3 Recommended Operating Conditions".
However the schematic for the TPS74801EVM-177 evaluation module shows the output capacitor as 4.7 uF.
Also the TPS748A-Q1 datasheet on the first page notes:
Stable with any output capacitor >= 2.2 uF
even though that same datasheet lists 10 uF as the minimum in table "6.3 Recommended Operating Conditions".
Does the TPS748A-Q1 differ from the TPS748A regarding the minimum output capacitor requirements?
Should 10 uF be considered the minimum required value for both even though the TI evaluation module is using 4.7 uF?