This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792: Watchdog timer when used with TPS25751.

Part Number: BQ25792
Other Parts Discussed in Thread: TPS25751

Tool/software:

Dear Sirs and Madams,

In the BQ25792 datasheet, the initial value of the watchdog timer is set to 40s.

When TPS25751 and BQ25792 are connected and used, will the watchdog timer setting be changed to Disable?

Also, I understand that the watchdog timer count is reset via communication.

In our configuration, we use the TPS25751 4CC task from an external MCU to communicate with the BQ25792 every 7 seconds, but do we have to reset the counter by manipulating WD_RST?

Regards,

Masashi