This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3823: High-level input current (IIH) of MR

Part Number: TPS3823


Tool/software:

Hi support team,

In the revision upgrade from SLVS165N to SLVS165O, the internal pullup resistor at MR of the TPS3823 was changed from 52kΩ to 90kΩ.
The high-level input current of MR remains -40μA (typ) and -60μA (max).
Is this correct?

Regards,
Dice-K