This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25798: bq25798 does not use battery

Part Number: BQ25798


Tool/software:

Hi Ti team,

The BQ25798 is currently used to charge a 1P3S lithium battery from a 12V adapter and supply power to the system. We are evaluating whether we can remove the battery and use only the 12V adapter to power the system with the current design. How should the BQ25798 be configured in this case?

  • Hi Yaoyi,

    The BQ25798 can be used without a battery and with charge enabled (i.e. CE pin = GND, CE bit =1 and no TS fault due to missing thermistor).  With charge enabled and only the minimum capacitance on BAT pin, the voltage at BAT will cycle between charge, OVP, termination, recharge, resulting in a triangle waveform.  The voltage on SYS follows BAT but never dips below MINSYS voltage.  With no battery connected it is recommended to disable charge with CE pin, CE bit or TS fault.

    Regards,

    Jeff

  • Hi Jeff,

    Thanks for your reply.

    One more question. Can the MINSYS voltage be increased through settings when there is no battery connected?

  • Hi Yaohi,

    Yes but the charger does not support MINSYS > VREG.  So the host must first increase VREG and then MINSYS.  VREG and MINSYS would have to be lowered before battery re-attach.

    Regards,

    Jeff