This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV61047EVM: input +12V, output +24V

Part Number: TLV61047EVM
Other Parts Discussed in Thread: TLV61047

Tool/software:

TLV61047 Evaluation Module

If I replace the following parts on the 595-TLV61047EVM-038, will the output be +24V?
Vin +12V


R2 1Mohm
R3 100kohm
L 10uH

Best,

Umino