Other Parts Discussed in Thread: 4213, BQSTUDIO
Tool/software:
Hello,
We need help resolving why only cell 1 is getting discharged much faster than the other batteries in the battery pack (13S 2P) when the pack is left in storage (@40% capacity). We use a 3rd party BMS that uses BQ78350-R1 with v1.03 firmware. It is not always happening, but 80% of the time, the battery stack gets shut down by BMS prematurely (in a couple of weeks) as it detects that Cell 1 has dropped voltage below the shutdown threshold. Cannot find any obvious reason why Cell 1 should drain faster. We have built many batteries and all of them show the same behavior.
Any help is greatly appreciated.
Thanks
Gamini