Other Parts Discussed in Thread: TPS74901
Tool/software:
Hi Team,
What is the maximum allowable pressure for the TPS74401?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
It also looks like there is a pin-pin newer part TPS74901, what is the maximum allowable pressure for that part?
Hi Nishka,
Max pressure depends on the package type. For which package option do you want these data for TPS74901?
Ishaan
The maximum recommended force is 20N uniformly applied to the top-side of the package perpendicular to the mounting surface.
Thanks! Is this information in the datasheet? I'm just seeing a few different similar questions here on e2e and I don't want to keep bother you all if its documented somewhere?
This information is not on the datasheet. We have to request this from TI packaging