Tool/software:
We are facing issues with a BQ24650 circuit and were able to repeat the problem on the bench.
We are charging 12V 7Ah lead acid using a 8W 18V MPPT panel.
In the morning, panel can be 14-17V for a while before the sun is fully up.
In this case, charger is enabled (STAT2 enabled), but not actually charging (voltage is below MPPT setpoint).
After 30 minutes, the charger disables (STAT2 disables) and does not enable again even if voltage becomes 18-21V.
Which timer/circuit/protection is this related to exactly? It seems like the pre-charge timer, but voltage on VFB is higher than VLOWV
We do not have control over the MPPSET pin, so cannot reset it with software.
Only solution seems POR after panel voltage is higher than the MPPT point, but lots of devices are already in the field.
Is this a known issue, what could be a fix?