This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A45: Design Review

Part Number: TPS7A45


Tool/software:

Hi,

We are using TPS7A4525 for generating  2.5V.Input voltage is 3.3V. 

Output current requirement is 1 A .

Kindly review the attached schematic and provide the feedbacks.

Regards,

Ashish

Review-3.pdf

  • Hi Ashish,

    The equivalent Cout required for stability is 10uF. After accounting for derating due to DC Bias and tolerance, please make sure a 22uF capacitor of 5V or higher rating is used in X5R or X7R types.

    Please make sure the current draw of both LDOs does not cause junction temperature to rise above 125°C. Follow the procedure described in section 11.3 of the datasheet.

    Regards

    Ishaan