Tool/software:
Hi
Could you help suggest materials that can provide LPDDR5X IC The current case has a 64GB requirement for ARL U/H and is evaluated with ARL-U/H 8533 Mhz
VIN = 20V or above
VDD2-CPU ICCmax is 4.15A
128Gb LPDDR5 VDD2 is 3.6A x 4ICS = 14.4A
Total VDD2 ICCMAX is about "18A"