Other Parts Discussed in Thread: BQ79600-Q1, , BQ79616
Tool/software:
Hello,
I have designed a custom PCB with a single BQ79616-Q1 balancing chip. The configuration in my test setup is 2 BQ79616-Q1 in a stack, communicating through a BQ79600-Q1 with a MCU (F280049) using SPI. Auto-addressing and waking the devices is successful, and I can read voltages and temperatures correctly.
However, I notice a buzzing sound coming from the PCBs with the BQ79616 devices. The frequency of this buzzing noise seems to depend on the rate with which I try to read the cell voltages, since requesting the data once every second produces a 'tick' every second, and increasing this rate to 100 times per second produces a buzzing noise.
Some things I noticed:
- Connecting only 1 BQ79616 device in my stack eliminates the sound. The sound is only produced when connecting a second device to the stack, and in that configuration both PCBs produce the buzzing sound.
- The daisy chain circuit is designed with capacitor and choke isolation, using recommended components mentioned in SLVAEP4. Removing the chokes on one PCB decreases the volume of the produced sound, but does not remove it completely.
- I found a thread which describes a similar observation: BQ79616-Q1: hear the buzzing sound when BQ79616-Q1 communicating - Power management forum - Power management - TI E2E support forums
Is this observation expected behaviour? Can it cause any harm or decrease in lifetime of the components? Is there a way to remove the sound? Thanks for the help.
Regards, Jeffrey