This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756: the chip lose its function

Part Number: BQ25756

Tool/software:

Hi,dear.

Sorry for coming here again.

I solve a problem previously,but a new problem is coming.

I connect the battery to my board and  connect a LED between RGEN and STAT1 that want to show the charger status.

After powering the board(about 50V), the LED is on showing the RGEN is right. But during I increase the voltage to 58V slowly , the battery connector pin is suddenly sparking twice. After that the LED is always off and I measure the RGEN, it is 0V. Obviously, the chip is bad.

How to judge the chip is good and how can I protect the chip from damage later?

Thank you!

  • Hello s sun,

    No problem at all.

    Thanks for being patient with this though. I am swamped at the moment. I'll get back to you early next week on this question.

    Best Regards,
    Ethan Galloway

  • HI,dear.

     According to your comments, I am full of anticipation that there will be good message to solve the problem of damage.

    Thank you!

  • hi,dear.

    To protect the chip from damage or spark, add a diode which can withstand higer voltage such as 150V between the chip and battery. Is it feasible?

    Thank you!

  • Hello s sun,

    Once again, thanks for being patient with this.

    To protect the chip from damage or spark, add a diode which can withstand higer voltage such as 150V between the chip and battery. Is it feasible?

    Yes, this is possible to do.

    How to judge the chip is good and how can I protect the chip from damage later?

    You can measure if the chip is good in a few ways. Here's the method I normally use:

    • Can the BQ25756 communicate over I2C when there is power on VAC or SRN?

    • When either EN_ADC=1 or the BQ25756 starts charging, does REGN come up to 5V?

    • Are the 10Ω resistors on SRN/SRP or ACN/ACP still 10Ω? Sometimes, a current surge can cause this resistors to break.

    • To test if the switching FETs are still good, I like using the diode measurement function on a multimeter to measure the FET from both drain to source and source to drain.

    I have a few questions to help debug the damage to your board:

    • Are those 10Ω resistors still good?
    • Is anything else on the circuit damaged?
    • Can you measure SW1 and SW2 with an oscilloscope once you have a working board again?
    • Does setting EN_CONV_FAST_TRANSIENT improve the circuit behavior?

    Let me know if you have any other questions about this.

    Best Regards,
    Ethan Galloway