This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25947: TPS25947

Part Number: TPS25947


Tool/software:

Hi.

i would like to use power protection switch - TPS259470ARPWR inside my design. i have three of those items on board. 

i don't need to use pin 3 named AUXOFF, it is listed as open drain output pin, hence didn't connected any pull up to it, it is left unconnected.

do i have a problem with the functionality of the IC?  or no problem at all. 

at page 36 it is listed as an output indicator, so i don't see any problem, but TI also wrote at page 37 this pin must be pulled up, maybe it meant only if we use it to drive other IC's, i would like to be sure.

please clarify on that.

thx.

Nitsan.