This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25751EVM: Error Flashing to Device

Part Number: TPS25751EVM


Tool/software:

Hi,

I’ve just started evaluating the TPS25751EVM board, but unfortunately, I’m unable to flash my configuration to the device.

Every time I attempt to flash, the progress bar reaches 10% before the following error message appears.

I’ve seen similar issues reported on the forum, where the device was detected as a “Microsoft” device instead of a “TI device”, and the flashing process failed accordingly

.

I have already tried the suggested solutions from those threads, including:

  • Using a different PC (Windows 10 instead of Windows 11)

  • Trying multiple browsers (Edge, Chrome, Firefox)

  • Swapping USB cables
    None of these attempts improved the situation.

  • Updated driver

Unfortunately, I only have one EVM, so I can’t verify whether the issue is specific to this board.

If you're familiar with this issue or have any suggestions, I’d greatly appreciate your support.

Thanks and best regards,
Raffael