This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6594-Q1: Pullup power rails for TPS65941319-Q1

Part Number: TPS6594-Q1

Tool/software:

Hi, 

The TPS65941319-Q1 PMIC User Guide for AM65 Sitara Processors has a table stating PMIC_nRSTOUT should be pulled up to VDA_MCU_1V8:

However, Figure 3-1 of the document shows the I/O supply pin, VIO_IN, being powered from a 3.3V rail:

This seems to contradict the datasheet for the TPS6594-Q1, which indicates nRSTOUT is within the VIO domain.

 

Since VIO_IN is powered by a 3.3V rail and nRSTOUT is within the VIO domain, shouldn't it be pulled up to VDD_MCUIO_3V3 instead of VDA_MCU_1V8?

Please advise. Thank you.