Tool/software:
Hi team,
- Is it allowed to connect E-load to TPS51200EVM?
- The VTTREF load is listed as a maximum of 10 mA, but the datasheet says min.10 mA | typ. 40 mA, and the upper limit is not specified in 4.1.3.
Is it OK to input up to 0.5W/0 .6V = 842mA for evaluation?
Also, is it correct that 0.5 W is just a limitation of the EVM?
![]()
Best regards,
Kazuki Itoh