Tool/software: Webench Power Designer
Hi.
I recently made a 30V-145V to 24V DC/DC power converter. I used the output from Webench as reference and made small changes to the circuit for my design. I have tried both the Webench design, as well as the modified design; both don't give any output. The Webench design led to burining of some components, while the modified design gave no output. I am attaching the transformer parameters, input and output waveforms for the modified design:
Transfromer parameters:
Lp = 19.0970 uH
Ls = 16.6053 uH
Laux = 3.95309 uH
Ns to Np = 0.933
Naux to Np = 0.455
Find the Webench design here.
The following are the transformer input waveforms. (Note that the attenuation of the probes ae set 10x the actual values: so take the values as 0.1x the readings)
The following are the auxiliary winding waveforms. (The attenuation is set at the right value here)
The modified designs have the following values for the parameters:
Rcs = 499 Ohm
Rqrt = 12 kOhm
Rqrb = 1.56 kOhm
Cd = 140 pF
Thanks and Regards