Tool/software:
I want to develop a battery pack with a capacity of 100Ah using 5Ah cells in a 3S20P configuration.
If I use bq40z50-r2, the maximum capacity is not suitable for 65Ah.
Can I adjust the scale factor to use it?
For example, reduce it to 1/10 so that 100Ah is expressed as 10Ah.
If possible, is it not necessary to adjust the current scale?
Thank you!