This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25750: BTST pins Diode selection

Part Number: BQ25750

Tool/software:

Hello There,

Today a colleague reviewed my schematic, and he noticed that I forgot the diodes on the BTST pins. 

Now I wonder if these diodes are necessary since table 6-1 in the datasheet indicates that the DRV_SUP pin functions as a gate drive supply, in my schematic I use the output of REGN as a gate drive supply.

If these diodes are necessary, special requirements need to be taken into account such as: the current through the diode, do they have to be schottky's, etc. The datasheet unfortunately does not go into this in more detail.

I am looking forward to your answers.

Kind regards,

Teun Noordkamp

  • Hello Teun,

    Now I wonder if these diodes are necessary since table 6-1 in the datasheet indicates that the DRV_SUP pin functions as a gate drive supply, in my schematic I use the output of REGN as a gate drive supply.

    Yes, these diodes are necessary for the BQ25750 to operate.

    do they have to be schottky

    Yes, the diode have to be schottky.

    The EVM uses the V1FM10-M3/H diode for the BTST diodes. I recommend making sure the that the reverse current through the diode is less than 100uA.

    Let me know if this answers your question.

    Best Regards,
    Ethan Galloway