Other Parts Discussed in Thread: TPS2121, , TPS25751, TPS25750
Tool/software:
Hi,
For our new product design requirements, when I saw this statement in your BQ25798 datasheet, I decided to add a TPS2121 feeding its VBUS, instead of using two pairs of ACFET-RBFETs, to ensure meeting our requirements for seamless transition between DC input sources:
To transition from one input to the other, the device first turns off the initially active ACFET-RBFET pair, waits until the VBUS voltage drops lower than VBUS_PRESENT, and then enables the new ACFET-RBFET pair. During this change over, the converter stops switching for a short period of time.
I'm still wondering if the two ACFET-RBFET pairs could have been fast enough to reliably work, but maybe with a lot of SYS capacitance?
Our product power:
•Battery: 2S
•Ext DC input jack: 10~15Vdc
Has priority over battery and USB-C input
•USB-C sink 15V, 3A (TPS25751D PPHV output)
•USB-C source: 5V, 2A (TPS25751D PP5V input)
•No OTG mode from BQ25798
•BQ25798 SYS feeds our system load:
17W ave, ~20W peaks
or 2.3A when SYS = 7.4V
•Reset occurs when SYS dips <~5.5V
For the BQ switch connection:
Ext DC jack -> BQ25798 VAC1/ACDRV1 NFET pair
TPS25751D PPHV -> BQ25798 VAC2/ACDRV2 NFET pair
Since VBUS_PRESENT could be 3.1Vmin, is there risk that SYS dips <5.5V, with battery not attached, when pulling the Ext DC jack source and switching to the USB-C (TPS25751D PPHV output)?
Would my current design using the TP2121 be less risky for our application to ensure no reset?
Ext DC jack -> TP2121 IN1
TPS25751D PPHV -> TP2121 IN2
(CP2 = 3.3V, PR1 = IN1/2, OUT -> BQ VBUS)
Thank you for your help!
Norbert