This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS24740: Looking for IC for hot swap and power oring

Part Number: TPS24740
Other Parts Discussed in Thread: TPS25947

Tool/software:

Like to find a TI IC that I can use, ideally multiples of a single chip.  I think TPS24740 may work, but it looks like you may have newer devices but wasn't sure if they support ORing.

Use case:

  1. ORing control for up to 4 power sources 10.6 to 16.6 @5A max each
  2. Will also have another source that is removable AC/DC 18v at 12A.  When this is connected I want to disable the other sources.  Could be a different ic for this, but would be nice to use the same chip.
  3. Inrush current limiting and time delay to allow for insertion time since all the hot swap pins are the same length.
  4. Blocking capability to charge the 4 sources when the external 18v source is connected, charge voltage will be 16.6V.