This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS929240-Q1: The reason of frame loss

Part Number: TPS929240-Q1

Tool/software:

Hi team,

The customer would like to know why frame loss occurs in the TPS929240 while the TPS929120 functions normally under the same settings. ( 1Mbps, DBWTIMER = 1ms)

What differences between them could have led to this situation? Currently, in the customer's application, the issue has been resolved by either sending each frame with an interval of more than 1ms or waiting for 1ms after detecting no response before sending the next frame. However, the customer still wishes to understand the root cause.

By the way, will the error in the following figure accumulation to the start bit of the next byte?

Regards,

Eileen