This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCG28826: 5V,3A Adaptor

Part Number: UCG28826


Tool/software:

Hello Ti support,

I am Chauhan Mihir and I am working in Aimtron technologies Pvt. ltd as sr. Hardware Design Engineer.

currently I am working on NPD in which we need to develop USB charger / Adaptor with below mention specification and certification.

List of required specification

  • Input voltage :- 90VAC to 270VAC
  • Input voltage frequency :- 50/60 Hz
  • Input current :- 1A
  • Output Voltage :- 5V
  • Output current :- 3A and 5A

List of required certifications.

  1. UL
  2. FCC
  3. CE
  4. IEC 60950-1
  5. UKCA
  6. NSW28222

Can we use "UCG28826" IC solution to fulfill our requirement?

If not then,

Kindly suggest us appropriate IC solution to fulfill our requirement with minimum no of components.

Regards,

Mihir