Part Number: UC3525A
Tool/software:
Hi Eric
What values of RT and CT should we choose for a fixed OSC output frequency of 190KHZ with an accuracy of 6% ? RD=0
In our current application, RT=4.22k and CT= 1.5nF, RD=0 , which gives a calculated value of 226KHZ (using formula for frequency, 1/[CT*(0.7*RT+3RD)]), but the actual measured value is 169KHZ on the board. Not sure why is this significantly different. We needed a fixed OSC output frequency of 190KHZ nominal (at UC3525AN PIN-4).
Regards,
N. Khan