This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650: Icharge

Part Number: BQ24650

Tool/software:

Hi,

Could you tell me the minimum ICHARGE that can be set?

Also, is it possible to connect Rsr=800mΩ and set Icharge=50mA?

Best Regards,

Nishie

  • Hello Nishie,

    The minimum charge current we recommend/validated is 0.5A with a 80mohm sense resistor. It may be possible to use a 800mohm sense resiistor, however the charge current accuracy might be very inaccurate. I recommend testing this on an EVM, to seen if this would suit your requirements

    What are you battery charging requirement? I can look for other suitable chargers.

    • Input Voltage?
    • Battery Voltage?
    • Host controlled or standalone?

    Best Regards,

    Christian.

  • Hi Christian-san,

    Thank you for your support.

    I will check the requirements.

    Best Regards,

    Nishie