Other Parts Discussed in Thread: LMR51610
Tool/software:
Hello,
In our projects, we are using the LMR51610 SMPS.
The IC enables when Vin is around 4.5V to 5V. I have connected the EN (Enable) pin to VIN through a 100k resistor.
Is it acceptable to use a 100k resistor, or should the EN pin be connected directly to VIN if we do not intend to use the UVLO function?
(In this case, R6 should not be placed, and R2 should be placed either with 100k or 0R)
Best regards,
Egemen