This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28C43: 15V-150V Vin Flyback Power Supply Design IC Recommendation

Part Number: UCC28C43
Other Parts Discussed in Thread: TIDA-01505,

Tool/software:

Hello,

I have linked the related question which is about TIDA-01505 reference design.

I want to ask this question also the power management forum.

Vin shall be between 15V-150V.

Vout shall be 12V and Iout shall be around 4A-5A.

Could you please recommend a IC that uses off the shelf transformer for our application?

Best regards,

Egemen

  • Hi,

    I do not think there are off-the-shelf transformers to meet your specs to what I know. A better way is that you ask the transformer vendors to see if they have or they can design one for you. UCC28C43 is ok to use and another similar device can do too, but no transformers off-the-shelf can be found - you have to ask the transformer vendors to help.