Tool/software:
Hi team,
I would like to ask the following two questions about the VIN pin and reset pin for LM63625DQPWPRQ1.
① :If the LM63625DQPWPRQ1's 12-, 13-pin VIN is unpowered and the 8-pin reset is pulled up externally to 3.3 V, is there any problem with the operation, performance, and lifetime of the IC?
②:In the case of ①, is there a possibility that the voltage of 3.3 V on the 8 pins flows backward to the VIN of 12,13 pins through the terminal protection diode inside the IC ?
Best Regard
Tomita