Tool/software:
I will be using two TPS629203-Q1. One will step the voltage down from 12V to 5V, the other will step the voltage down from 12V to 3.3V. I would like to use the Auto PFM/PWM with AEE setting for better performance at light loads. However, there is a concern that these regulators may be operating at the same frequency, causing EMI noise concerns. Is there a recommended configuration for using two of the regulators?