This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: Can multiple 4s2p cell packs be placed in parallel with each pack having its own BQ40Z80 BMS and then there own BQ24617 for charging

Part Number: BQ40Z80
Other Parts Discussed in Thread: BQ24617

Tool/software:

Can multiple 4s2p cell packs be placed in parallel with each pack having its own BQ40Z80 BMS and then there own BQ24617 for charging and then charging them from a common external power supply with the appropriate current rating (say 3A per pack)  What are the pros and cons and the pitfalls to avoid?  Is there a better way to do this?  Can all of the outputs be tied together to run the load?