Tool/software:
Hi TI support team,
I have created a case CS2614626 before and I still have some questions need to follow with you.
Below introduced my request.
We have conducted a test that when we connect the 24V voltage to A point under 125degC, we measured the voltage on B point is 8V. We checked the reverse leakage current of Diode under 125degC is 2mA, so 24V will flow through Diode and pull up the voltage level on point B. We have tried replacing the diode with 4uA reverse current under 125degC to do short to battery test and there is no issue for the output of LDO. So, if we know the capability of LDO reverse leakage current, it will support us to do Diode selection.
You have given me below reply last time.
It did help, thanks a lot. But it cannot support us to choose suitable diode to limit the reverse current flowing into LDO. Is that possible to help to do test or simulation to get the LDO reverse current capability? Please help to check and let me know if any unclear. Thanks.
Hi Pengpeng,
As mentioned in my earlier email, the max Vout for this device is 7V. So, setting the LDO Vout to 8V likely damaged the device and so the test results are not in line with expected.
Reverse leakage current and quiescent current are two separate current paths. You cannot use the attached figure to determine leakage current.
Upon checking, this part does not have internal reverse current protection, we don't spec out the max reverse leakage current. A good rule of thumb is to limit it to less than 5% of the Iout which would be 7.5 mA.