Tool/software:
Hello,
My customer has the following inquiry regarding the use of TPS548A28:
Q1. If you has any data to confirm output current derating for TPS548A28, please provide it.
Q2. They want to use TPS548A28 under the following conditions.
- VIN = 12V, VOUT = 3.3V, IOUT = 9A(max)
Is there any expected issue if the internal temperature of the system is high and the device temperature is used above 100 degrees Celsius (Not above 125 degrees Celsius)?
Thank you.
JH