This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: BQ40z80 not detecting on certain connection process

Part Number: BQ40Z80


Tool/software:

Hello, 

I am facing issues while making a battery pack of 4S BMS designed in house.
Scenario 1: connect the cell terminals of the battery then the power through connector, it works no issues.
Scenario 2: connect power then cell terminals it doesn't work
Scenario 3: connect cell terminal then positive/negative and then the remaining one, doesn't work
The cell terminal doesn't power on the board, the last cell isn't common or net tie with the pack +. This is made intentionally.
Is there a sequence on how to connect it ?