Tool/software:
The CAD footprint provided on the TI webpage does not seem to match the datasheet specification:
Pads 1,7,8, and 14 are 0.355^mm wide - the datasheet suggests 0.5mm
The pitch between pads 6 and 7 is 0.65mm - the datasheet says it's 0.725mm
There are no thermal vias.
The datasheet does not provide the dimensions for the "tabs" at the top and bottom of the thermal pad but they appear to be symmetrical. In the CAD footprint their dimensions are different. If the thermal pad is symmetrical these tabs would be (4.6-2.5)/2=1.05mm in the y dimension. I can't find this detail on the datasheet - please confirm.
Thanks.