This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: Short circuit discharge time over

Part Number: BQ40Z80


Tool/software:

Hello,

I have configurate the ASCD to have 0µs to detect the short circuit discharge with a current of 33.3A. i have a shunt of 1mohm.1526.Gauge after temp.gg.csv

But the delay to detect the short circuit is 360µs.

Without the capacitor C1,C2 and C3, the time to detect the short circuit is 300µs.

How can i have a detection at 0µs.

Thanks,

Best Regard,

Ludovic Micou