Tool/software:
Hi team,
Is there absolute max ratings for the pulsed current for this device at OUTA and OUTB for VDD=15V?
regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi team,
Is there absolute max ratings for the pulsed current for this device at OUTA and OUTB for VDD=15V?
regards,
Hi Tsuji-san
Responses will be delayed due to US holiday.
Our dedicated expert will get back to you shortly.
Regards,
Hiroki
Hi Tsuji-san,
Thanks for your patience.
For peak current, the device is rated for 4A source and 6A sink maximum current.
For operating current, you can refer to the 5.7 Safety Limiting Values specifications and 5.10 Insulation Characteristics Curve that contains safety limiting current values for the device. Exceeding these values will have an effect on performance.
Regards,
Hiroki
Hello Honda-san,
Thank you for your response.
It seems 4A source and 5A sink are typical value.
Is there maximum value such like Absolute maximum ratings which impact product reliability if user exceeds its max limit?
regards,
Hi Tsuji-san,
The 4A source and 6A sink currents are the points at which the device saturates.
The current may be able to reach higher values if pushed but it may lead to saturation under corner cases which will lead to increased losses in the gate driver's internal pull-up and pull-down FETs. The design should avoid exceeding these values to prevent this from occurring.
Hope this is helpful!
Regards,
Hiroki