This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63710: Is it possible to meet EN55022 requirement ?

Part Number: TPS63710


Tool/software:

Dear Specialists,

My customer is considering TPS63710 instead of LTM4651 and has a question.

I would be grateful if you could advise.

---

I am considering replacing the power supply I am considering using LTM4651 with TPS63710.

・Vin=9V
・Vout=-2.8V
・Imax=600mA
・It is for an op-amp that amplifies the analog signal of the optical sensor and inputs it to the AD converter.

The LTM4651 features low noise and meets EN55022B requirement.

Can TPS63710 be also made EN55022B compliant?

If the TPS63710 satisfies EN55022, then it is possible to consider it for replace.

I would appreciate any comments on whether it is possible to replace it and any points to note.
If it can be replaced, there will be a big cost advantage.

---

I appreciate your great help in advance.

Best regards,

Shinichi