Tool/software:
Hello,
In the datsheet it is recommended to have input capacitance of 3uF (after considering derating factor).
Due to design constraint I have only two MLCC 2.2uF 100V and after considering derating factor effective is only 1.1uF (including both).
I think it is fine to consider this design. Do you recommend more capacitance? If yes,could you please provide more explanation.
Vinmin: 8V
Vout: 6.3V
Ioutmax: 0.5A
fsw: 500kHz
Thank you,