This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: RSOC

Part Number: BQ40Z50-R1

Tool/software:

Hi

Customer has a question

The original Max Error was 1% and then entered SHUTDOWN mode After a period of time, the Max Error of charging wake-up will have a chance to change to 2% What is the reason for this? Just reset it and it will return to normal. Or charge and discharge it once more and it will return to normal.