This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCG28826: Vin:90V-264V, Vout:12V/4A with cable AWG 16 120cm, efficiency over 90%

Part Number: UCG28826


Tool/software:

Hello expert,

May I know if there is UCG28826 could be used in below requirement? Thanks a lot!

Condition : 

Vin:90V-264V, Vout:12V/4A with cable AWG 16 120cm, efficiency over 90% at 4 points loading.(10%/25%/50%/100% loading)

Best regards,

Ann Lien

  • Hi Ann,

    Yes, device can support 12V/4A for an input voltage range of 90V to 264V AC, but please can you clarify that by AWG 16 120cm, you mean you want to use single strand of AWG 16 wire of 120cm length to make transformer primary winding?

    Also, if possible, please provide more details of transformer design like which transformer core are you planning to use.