Other Parts Discussed in Thread: LMR50410-Q1, LMR50410, LM5166
Tool/software:
Trying to create a design using the Type 3 Ripple Generation Method using the LMR5166-DESIGN_CALC_REVA1 calculator.
(1) The LMR516XX-DESIGN_CALC_REVA1 refers to the LMR50410-Q1 device. Is this correct?
(2) The Type 3 Ripple Generation method uses RA, CA and CB parameters not shown in the figure.
(3) Should the output capacitor chosen include downstream capacitors such as input capacitors
for other regulators and local capacitors for processors and the like?