This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27520-G4: I2C communication speed

Part Number: BQ27520-G4


Tool/software:

Dear Sirs and Madams,

We are considering using the BQ27520-G4.

We would like to confirm the I2C specifications for communicating with an external MCU.

I have confirmed that the BQ27520-G4 datasheet specifies the I2C clock frequency as 400kHz (max).

In I2C fast mode, 400kHz operation is common, but I think that tolerances are taken into consideration.

For example, 400kHz +/- XX kHz

Is there any tolerance for error regarding this 400kHz (max)?

Regards,

Masashi