Tool/software:
Hi,
In one the custom board I am using LM73100 as the oring device for 2 USB inputs. The problem is the Power good output signal, Normally it works properly as per design. But sometimes the PG signal goes low even if the input is 5.03V and output is 5.02V. Dont know the reason. After couple of times, we remove the USB cables and then it starts working normally. Any idea what can be the issue. I have attached schematic section of LM73100.