This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55340: TPS55340 : error when running in Simetrix

Part Number: TPS55340


Tool/software:

Hello,

I'm trying to make a simulation for TPS55340 Boost converter in Simetrix 9.10.

After importing the *.lib file contained in the SLVM589A folder, I'm able to import and create a symbol for the component.

But the transient simulation fail when I try to run it.

It gives the following errors :

*** WARNING *** Model 'TPS55340_TRANS.R_U8_R3': Unknown parameter 'DEV'
.model R_U8_R3 RES R=1 DEV=47%

I tried to delete the "DEV=47%" then I got another error :

design.net (12): ...
*** ERROR *** Error in declaration of parameter 'SS'