This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25750: USB PD 100W (20V/5A) and 240W (48V/5A) Power Input Solutions

Guru 12115 points
Part Number: TPS25750

Tool/software:

Hi,

  1. USB PD 100W (20V / 5A) Power Input Configuration
    The customer intends to drive a printer head that previously faced power limitations. They are considering using USB PD (up to 100W) for power input.
    Could you kindly suggest a total solution including the USB PD controller, power path devices, and necessary protection components?

  2. 48V / 5A (240W) Power Input Configuration via USB PD (PD 3.1) or DC Input
    The customer is also interested in evaluating a 240W solution, ideally via USB PD 3.1 (EPR) if supported.
    Please let us know if any TI solution is available for this use case. If not, a 48V DC-input-based configuration using TI controllers or power ICs would be appreciated as an alternative.

Best regards,
Conor