Tool/software:
Hi team,
Our customer is considering this device by USB BC1.2 supply on Type-C connector.
They have few question about this I2C control behavior.
1. Can this device control to fix SYS output from BAT path only or VBUS path only by registor change from CPU?
If it is possible, does Dynamic Power Management still have priority?
2. In this device SDP current limit is 500mA. If we need support USB100(current limit 100mA), is it possible by REG0x06_Input_Current_Limit Register setting?
3. Concern with question 2, recentry is it not require to support USB100? Is the trend only USB500 support in the case of USB BC 1.2 system in the world market?
Best regards,
teritama