The TPS7633 data sheet states that the part has no minimum output current requirement, however in my board it doesn't regulate unless I throw a dummy load of about 7KΩ or less from the output to ground. Obviously, pulling 470uA just to get it to regulate negates the reason I designed the part in to begin with, namely its very low quiescent current.
My board is currently unpopulated except for the regulator and a few discretes. I have a 10UF tantalum (3Ω ESR) right at the regulator output and four or five 100NF 0603 ceramics scattered around the board. I see no signs of oscillation from the regulator, but if I have more than 7K ohms across the 3.,3V output, the output voltage pretty much just follows the input: 9V in= 9V out. I'm glad I checked before putting in the 3.3V IC's :-)
What am I missing?
Thanks,
Julia