Hi,
I'm using a TPS5410 in my design to regulate to 17V from input voltage of 28V.
Circuit is right from the data sheet, feeback resistor values 15K and 1.13K. Layout also very close to datasheet. Output filter cap is 100uF Panasonic EEE-HA1V101
I'm finding that sometimes I can get a condition where the output voltage does not come up. Sometimes it recovers after a small time, other times it stays low (at about 1V output) for good. I can see the out attempting to start up every 25mS for a burst of pulses for about 500uS.
I tired fiddling with the output cap and adding some feedback compensation as outlined in slva237 but had no effect.
I did observe that if I add a 0.5 ohm resistance in series with the output before my load then the issue goes away. My load is basically about 10 opamps with scattered bypass caps. Current draw is about 75mA at 17V.
Any Ideas?